Solution 14800: Replacing the Battery in a TI-1706 SV.
How can I replace the battery in a TI-1706 SV?
The TI-1706 SV is dual powered. It is solar and battery powered to work anywhere. The TI-1706 SV uses one LR54 (1.5V) alkaline button cell battery.
About replacing the cell battery on a
TI-1706 SV:
For safety purposes and to
prevent ingestion, the button-cell batteries in school and student-owned
calculators as well as basic/elementary calculators without battery doors are
not designed to be replaced. It is possible to replace the battery by removing
the back case of the calculator, but opening the back of the calculator voids
the one-year, limited warranty. This must be done carefully, as we cannot be
held responsible for any damage caused when you attempt to replace the battery. If your calculator is already out of warranty, you might choose to
remove the back case to replace the battery
To replace the button-cell battery:
• Using a small Phillips
screwdriver, remove the screws that are on the back of the calculator.
• Carefully
pry apart the back case and the front case. Be careful not to damage any
internal parts.
• Remove the lithium battery carefully and replace it with a
new one.
Safety precautions:
• Avoid contact with other
calculator components while changing the battery.
• Properly dispose of the
used battery immediately.
• Do not leave batteries within the reach of
children.
• Do not incinerate batteries.
If your calculator does not power on, please see Warranty Information on Texas Instruments Products Purchased in the United States and contact TI-Cares to obtain service information.