Solution 40317: TI-30XS MultiView™ and TI-34 MultiView Scientific calculator battery information.
What type of battery, and how to remove or replace the battery on a TI-30XS Multiview and TI-34 MultView Scientific calculators.
The TI-30XS MultiView™ and TI-34 MultiView scientific calculators both use one 3 volt CR2032 lithium button cell battery.
About replacing the button cell battery on a scientific calculator:
For safety purposes and to prevent ingestion, the button-cell batteries in school- and student-owned calculators without battery doors are not designed to be replaced. It is possible to replace the battery by removing the back case of the calculator, but opening the back of the calculator voids the one-year, limited warranty. This must be done carefully, as we cannot be held responsible for any damage caused when you attempt to replace the battery. If your calculator is already out of warranty, you might choose to remove the back case to replace the battery.
To replace the cell battery:
- Remove the protective cover and turn the calculator to face downwards.
- With a small screwdriver, remove the screws from the back of the case.
- From the bottom, carefully separate the front from the back. Be careful not to damage any of the internal parts.
- With a small screwdriver (if required), remove the battery.
- To replace the battery, check the polarity (+ and -) and slide in a new battery. Press firmly to snap the new battery into place.
- Important: When replacing the battery, avoid any contact with the other components of the calculator.
- Dispose of the dead battery immediately and in accordance with local regulations.
Battery precautions
- Do not leave batteries within the reach of children.
- Do not mix new and used batteries. Do not mix brands (or types within brands) of batteries.
- Do not mix rechargeable and non-rechargeable batteries.
- Install batteries according to polarity (+ and -) diagrams.
- Do not place non-rechargeable batteries in a battery recharger.
- Properly dispose of used batteries immediately.
- Do not incinerate or dismantle batteries.
- Seek Medical Advice immediately if a cell or battery has been swallowed. (In the USA, contact the National Capital Poison Center at 1-800-222-1222.)
Battery disposal
- Do not mutilate, puncture, or dispose of batteries in fire. The batteries can burst or explode, releasing hazardous chemicals. Discard used batteries according to local regulations.
- Per CA Regulation 22 CCR 67384.4, the following applies to the button cell battery in this unit: Perchlorate Material - Special handling may apply. See www.dtsc.ca.gov/hazardouswaste/perchlorate
If your calculator does not power on, please see Warranty Information on Texas Instruments Products Purchased in the United States and contact TI-Cares to obtain service information.
Last updated: 6/14/2024