Solution 12250: Calculating a Hyper Geometric Probability Distribution on the TI-30X IIS/B.
How do I calculate values for a hyper geometric probability distribution on the TI-30X IIS/B?
There is not a pre-defined function on the TI-30X IIS/B that will find the statistical values for a hyper geometric probability distribution. However, the formula can be entered to find the results. The example below will demonstrate how to find p(1) of a hyper geometric probability distribution.
Example:
What is P(1) if,
N = 12
n = 4
k = 3
Since P(x) = {C(k, x) *C(N-k, n-x)}/C(N, n)
With substitution, P(1) = {C(3, 1) *C(12-3, 4-1)}/C(12, 4)
The values will be input into the TI-30X IIS/B as follows:
1) Input [(] [(] [3].
2) Press [PRB].
3) Scroll to nCr using the directional arrows. (There will be a line under nCr indicating that function is selected)
4) Press [ENTER].
5) Input [1] [)] [(] [9].
6) Press [PRB].
7) Scroll to nCr using the directional arrows and press [ENTER].
8) Input [3] [)] [)] [÷] [1] [2].
9) Press [PRB].
10) Scroll to nCr using the directional arrows and press [ENTER].
11) Input [4] then press [ENTER].
The displayed answer will show 0.509090909
Please see the TI-30X IIS/B guidebook for additional information.