Solution 11470: Canceling Transfers on the TI Connect™ Software for Windows®.
How do I cancel transfers within the TI Connect software?
There are two options to canceling transfers within the TI Connect software. Transfers can be cancelled when the current data file is done sending or transfers can be cancelled immediately (in the middle of a data file sending).
*Note: A transfer refers to any exchange of information between the calculator and computer, including a copy, move or send.
1. To cancel after the current transfer completes:
Click Cancel. The name on the cancel button changes from Cancel to Cancel Now, and the transfer continues until the current data file completes its transfer.
2. To cancel the transfer immediately:
Click Cancel. The name on the cancel button changes from Cancel to Cancel Now.
Click Cancel Now and the transfer ends immediately.
For more information and help using the TI Connect software, open TI Connect and click on the "Help" radio button located in the bottom right-hand corner.