Solution 34694: Using the fInt Function Integral Command on the TI-84 Plus Family of Graphing Calculators.
How do I use the fnInt Function Integral command on the TI-84 Plus family of graphing calculators?
The fnInt command returns the numerical integral of an expression with regards for real numbers only. The numerical integral is based on the Gauss-Kronrod method. The numerical integral is calculated with respect to the variable, given a lower limit, upper limit and a tolerance. Tolerance is optional and if not specified it is defaulted to 1E-5. The TI-84 Plus family of graphing calculators display a template when in MATHPRINT MODE but while in this model Tolerance cannot be entered.
When in CLASSIC mode, the syntax for the fnInt command is below:
fnInt(expression, variable, lower, upper[,tolerance]), between lower and upper, with specified tolerance.
Example: Find the function integral of A2, for the variable A, with 0 as the lower bound and 1 as the upper bound using the MATHPRINT mode:
1) Press [MATH] then [9] to select 9:fnInt(
2) Press [0] [→] [1] [→] [alpha] [math] [x²] [→] [alpha] [math] [enter]
In CLASSIC mode, follow the steps below:
1) From the main screen press [math] then [9] to select 9:fnInt(
2) Press [alpha] [math] [x2] [,] [alpha] [math] [,] [0] [,] [1] [)] [enter]
Please see the TI-84 Plus Family guidebooks for additional information.
Last updated: 7/23/2024