Solution 12027: Detailed Information Provided When Using the Catalog Stopped After OS Update on the TI-83 Plus Family, TI-84 Plus Family, and TI-Nspire™ in TI-84 Plus Mode.
I used to be able to get more information on commands in the catalog, however since I upgraded operating systems I cannot. How do I change it so that I get more information?
The detailed information provided in the CATALOG menu of the TI-83 Plus family, TI-84 Plus family, and TI-Nspire in TI-84 Plus mode is provided by the Catalog Help App. When an OS (Operating System) update is performed, the RAM is cleared, and all running applications are stopped.To restart the Catalog Help:
• Press [APPS].
• Use the arrow keys to navigate to CtlgHelp and press [ENTER].
This will start the App.
Note: If an error message is received indicating "ERR:Version" verify that the latest release is in use. The current version is 1.1 which may be retrieved from Software, OS Updates and Apps.
Please see the TI-83 family and TI-84 Plus family guidebooks for additional information.
TI-Nspire in TI-84 Plus mode users may use the TI-84 Plus guidebook.