Solution 40158: Transferring the TI-84 Plus CE Bundle version 5.6.0.20 displays the error "Not for you" using TI-Connect CE 5.4.0.1181.
Why does the TI-84 Plus CE Bundle version 5.6.0.20 displays the error "Not for you" while transferring using TI-Connect CE 5.4.0.1181?
The TI-84 Plus CE Bundle version 5.6.0.20 includes files for all models of
Texas Instruments CE family calculators:
TI-84 Plus CE
TI-84 Plus
CE-T
TI-83 Premium CE
The bundle can only transfer files which are
compatible with your model of TI-84 Plus CE.
The "Not for you" error is just indicating that some of the files are not
compatible.
You will need to click [OK] 4 times to dismiss the dialogs
that appear to allow the installation to proceed. The 4 files below will display
this
error:
GRAPH.8xv
LINREGR.8xv
TISTEMEN.8xv
TISTEMFR.8xv
Please Note: A “Python” App and “Hello” program
will be transferred to the TI-84 Plus CE calculator but will not be functional.
If you find either of these to be intrusive you can remove them using the steps
below:
1) First to delete the "Python" App press [2nd] and then the [+] key
to access the memory menu.
2) Press [2] to access "2: Mem
Management/Delete"
3) Press [alpha] then [math] to access the "A: Apps" menu.
4) Use the [Arrow] keys to move the cursor in front of the "Python" app then
press [del] then [2] to select "2:Yes".
5) Press [clear] and wait for the
defragmentation process to complete.
6) Next to delete the "Hello" program
press [2nd] and then the [+] key to access the memory menu again.
7) Press
[2] to access "2: Mem Management/Delete"
8) Press [alpha] then [apps] to
access the "B: AppVars" menu.
9) Use the [Arrow] keys to move the cursor in
front of the "Hello" program then press [del] to delete the program.