Solution 37817: What are the capabilities of the TI-Innovator™ Hub I/O Modules available from TI?
What are the capabilities of the TI-Innovator™ I/O Modules?
TI-Innovator Hub™ I/O Module Details
What are the capabilities of the TI-Innovator™ I/O Modules available from TI?
What other I/O Modules could work with the TI-Innovator™ Hub?
The items contained in the TI-Innovator™ kits have all been verified to be fully compatible with the TI-Innovator™ system. The sketch of the TI-Innovator™ Hub can support other modules that are compatible with the universal 4-pin connector that is used for the input and output ports. Supported commands and potential modules are listed below. If there are specific components you think would be valuable for classroom activities, please contact TI-Cares and provide your feedback.
Please Note: Texas Instruments Customer Support is available to answer questions about the products that are sold directly through our Educational Products Dealers or the TI Online Store. For components purchased elsewhere, such as those listed below, please refer to the manufacturer or point of purchase for technical support.
Example Module Component(s) |
Command/Sketch Object |
Barometer Sensor |
BAROMETER |
Button, Magnetic Switch |
BUTTON |
3-Axis Digital Compass |
COMPASS |
Fan |
DCMOTOR |
Temperature & Humidity Sensor |
DHT |
Single or variable color LEDs |
LED |
Light sensor |
LIGHTLEVEL |
Sound Sensor, Loudness Sensor |
LOUDNESS |
Moisture Sensor |
MOISTURE |
Collision Sensor |
MOTION |
PIR Motion Sensor |
MOTION |
Slide Potentiometer |
POTENTIOMETER |
Rotary Angle Sensor |
POTENTIOMETER |
Electromagnet, Relay |
RELAY |
Servo Motor |
SERVO |
Buzzer, speaker |
SPEAKER |
Switch |
SWITCH |
Temperature Sensor |
TEMPERATURE |
For more details refer to the TI-Innovator™ System eGuide. To access the eGuide, please click on [View]. If you require further assistance please contact TI-Cares for support at 1-866-846-2844 or Send us an E-Mail.