Solution 32012: Using the Update Class Roster Feature in the TI-Nspire™ Navigator™ Teacher Software.
How do I use the update class roster feature in the TI-Nspire Navigator Teacher Software?
To use the update class roster feature in the TI-Nspire Navigator Teacher Software follow the steps listed below:
Please Note: If you are attempting to use a .csv or .txt file created for a version of TI-Nspire Navigator Software earlier then 3.2.0.1212 you will need to update this file with the information listed in Knowledgebase Article #32011.
• In the TI-Nspire Navigator Teacher Software click [Window] [Class Workspace]
Please Note: Items with an asterisk are required however items without an asterisk can be left as [Blank] since they are not required.
• On the next screen you will receive a message that your classes were completed successfully, click [OK] to close the wizard.
If you need additional assistance with other components of the TI-Navigator System please visit Knowledgebase Article #31211.
If you require additional assistance please contact TI-Cares.